version française - Who are we? - Customer services - International - Contact

Mechanical components by mail order

Mechanical components by mail order

Home - Technical files - Fixings - Ways of fixing toothed wheels - Attachment by clamp assy

   Track customer order :  

Attachment by clamp assy

Principle

By tightening the screws, the user deforms a conical ring, and causes a strong force between the shaft and bore. The liasion obtained is complete and rigid (i.e. recoil-free) , and easily removed.

ensemble de serrage  schéma fixation ensemble de serrage

Advantages

By avoiding the manufacturing accidents which can be caused whilst cutting keyways etc… This system actually increases the sectional strength of the shaft and decreases both the concentration of stress points and the phenomenon of metal fatigue cracking.

 

For equal diameters, the transmissible torque with this method is much higher. Work to be done on the shaft and bore is limited to insuring an H8/h8 tolerance and a surface finish of at least Ra=1,6mm for self-centering assemblies (RT25 and RTL450).

 

A guide should be envisaged for the other assemblies. These locking assemblies are recommended for all types of toothed wheels, and especially for pulleys, sprockets and gears with large pitches or important modules.

Back to Ways of fixing toothed wheels

Back to Fixings

Back to the list of technical files

Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact

copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+

Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland

mechanical drivesconveyor partspower transmissionlinear drives
linear motionrotary motiongears