version française - Who are we? - Customer services - International - Contact

Mechanical components by mail order

Mechanical components by mail order

Home - Technical files - Fixings - Ways of fixing toothed wheels - Attachment by key

   Track customer order :  

Attachment by key

Principal

The use of a key makes it possible to make a connection by blocking a rotation. It requires the machining of a groove in the shaft and bore. For manufacturing to be possiible, the groove to be realized in the bore must emerge on both sides.

A parallel key is a rectangular piece of metal, embedded half and half into the shaft and hub. The machining of the groove in the shaft is effected with the aid of a two-bladed cutting tool.
A keyway of this type is excellent for the transmission of high torque levels.

To find out more about the machining dimensions

clavette->  schéma de fixation par clavette

Disk (or half moon) keys are used for the transmission of weaker torques. The machining of the keyway into the shaft is very easily done using a three bladed cutter.

 

A keyway does not stop axial movement of the system. Therefore it must be combined with another locking system, such as a thread and bolt (circlips).

clavette demi lune->  schéma de fixation par clavette demi lune

Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact

copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+

Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland

mechanical drivesconveyor partspower transmissionlinear drives
linear motionrotary motiongears