version française - Who are we? - Customer services - International - Contact

Mechanical components by mail order

Mechanical components by mail order

Home - Technical files - Fixings - Ways of fixing toothed wheels - Attachment with circlips

   Track customer order :  

Attachment with circlips

Principle

Circlips stop axial movement between two components.
There are two types of circlips, one for shaft mounting and one for inside the bore.

Usage

This requires a groove to be cut into either the bore or the shaft. They are then fitted axially, from one end of the shaft or bore with the aid of a specialised tool.

 

Note: a minimum (or maximum) clearance diameter is needed for the installation.

circlip externe
circlip interne
schéma de fixation par circlip

The use of these components is often associated with a keyway in the assembly of pulleys or spur gears.

Back to Ways of fixing toothed wheels

Back to Fixings

Back to the list of technical files

Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact

copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+

Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland

mechanical drivesconveyor partspower transmissionlinear drives
linear motionrotary motiongears