- Who are we? - Customer services - International - Contact
Mechanical components by mail order
Mechanical components by mail order
Home - Technical files - Fixings - Ways of fixing toothed wheels - Attachment by locking ring
Attachment via a locking ring is a fast and efficient method of attaching all types of toothed wheels. Two solutions exist, locking with half a locking ring (type CT), or locking with the aid of a full collar (CC).
This first solution involves the machining and removal of half of the gear hub and the piercing of two threaded holes in the rest of the hub.



The other solution involves trimming the hub and the machining of two channels - as shown in the diagram.



In both cases, the result is a completely rigid joint, which is perfectly suited to the transmission of high levels of torque
Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact
copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+
Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland
mechanical drives • conveyor parts • power transmission • linear drives
linear motion • rotary motion • gears