- Who are we? - Customer services - International - Contact
Mechanical components by mail order
Mechanical components by mail order
This system permits an important reduction ratio. In certain conditions the system is irreversible. The efficiency of this system is low but increases in relationship with the lead angle of the teeth. The direction of the helix is the same for the worm and the wheel.
There is no standardisation for worms and wheels. In the case of a breakage, the defective element must be replaced with an absolutely identical model. Most of the time, this will have to be custom-made. Indeed, each manufacturer chooses the worm diameter he likes. This has an influence on the Helical Angle, the Pitch Diameter and the centre to centre distance.
As their name indicates, these wheels allow the absorption of the recoil which would exist in a classical worm and wheel setup. Springs are placed in channels between two wheels of the same dimensions, which are attached together with a circlip. On assembly, the two discs should be offset by a few degrees, this compresses the springs in order to allow them to absorb the recoil.
Attention, Anti-recoil wormwheels can be only used with Single Start worms.
Yes, we can custom-produce couples of worms and wheels. Contact us on: +33 (0)437 496 496.
For worm screws
Four principal parameters characterise a worm
These parameters are bound by a complicated mathematical relation.
The helix angle is difficult to control. The direction of slant of the teeth is done visually: hold the screw in driving position: when the nets go up towards the line, threading is tilted to the right, and when they go up towards the left, threading is tilted to the left.
![]() |
![]() |
| Left hand threaded | Right hand threaded |
To measure the thread, take the dimension of a top of a start at the following start.

To control the number of starts, it is necessary to look at the starting number of starts (to look at the screw in the axis, or vis-a-vis with boring).
![]() |
![]() |
| Don't count the starts like this | They should be counted in this direction |
For the wheels for worms
Four principal parameters characterise a wheel
The first three parameters are bound by the mathematical relation
de = m x (Z+2) or m = de/(Z+2) or Z = (de/m)-2
The determination of the slant direction of the teeth is made visually (put the gears flat on a table: if the teeth go up towards the line, the teeth are tilted to the right, if the teeth go up towards the left, the teeth are tilted to the left.
The helix angle is difficult to control. The only way is to put the wheel with the worm that was made for it (even module and even number of starts).
![]() |
![]() |
| This screw with four starts cannot function with this wheel planned for a single start. | On the other hand, this wheel and this screw are compatible |
Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact
copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+
Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland
mechanical drives • conveyor parts • power transmission • linear drives
linear motion • rotary motion • gears