- Who are we? - Customer services - International - Contact
Mechanical components by mail order
Mechanical components by mail order
All the gears manufactured by HPC are made to H8 tolerance.
Other tolerances, such as H7 for example, are not possible.
The tolerance of the outside diameter is +0/-0.15mm.
The concentricity is 0.1mm and the perpendicularity is11.
The centre to centre tolerance is +0/+0.05mm.
The gears are not rectified. The condition of the surface is Ra=3.2.
HPC's product line is presented in a catalogue with around 35,000 parts as standard. Nevertheless, they can be easily modified, or even custom-made from a design or model, to fill a particular need.
Yes, it's a service we are frequently called upon to provide.
In the case of a broken or damaged gear, send it to us. Our technicians will then be able to determine the dimenensions. For helical gears it is always preferable to send us both wheels at the same time: certain information can then be,gained from either one or the other component, this is very important with worm and wheel systems.
HPC has a catalogue with numerous standard wheels, with pre-defined dimensions. However, certain dimensions can be modified in order to adapt a part to your system. The most common modifications are reboring or the addition of a keyway, pinhole or threaded hole. Thermal processing is also possible. HPC can, on request, modify its standard range to adapt them to your needs.
For this service, talk to our technicians on +33(0)4 37 496 496 or fax us a rough sketch on +33(0)4 37 490 055.
Actually, there are two PAs in existence. The angle of 14°30' was widely used in the past, but nowadays is a lot less common. It is sometimes used for Imperial componants. The angle of 20° has become much more commonplace. It's therefore impossible to say if one or the other is better, however it is clear that the 20° PA is used much more often for metric modules.
Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact
copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+
Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland
mechanical drives • conveyor parts • power transmission • linear drives
linear motion • rotary motion • gears