- Who are we? - Customer services - International - Contact
Mechanical components by mail order
Mechanical components by mail order
There is a progressive meshing, thanks to the inclination of the teeth. The number of teeth engaged at any one time is higher, which assures a continuous mesh.
The transmission obtained is thus smoother and quieter than can be obtained from a spur gear.
A parallel helical gear with the teeth inclined to the right will mesh with a parallel helical gear with the teeth inclined to the left if both gears have the same angle of inclination (HA -helical angle). The latter is not standardised, and can vary from one manufacturer to another. HPC offers standard gears with an HA of 17°45'. The HA has an effect on the pitch diameter (PCD), a parallel helical gear is not interchangeable with just any other old helical gear.
This type of gearing permits a change of direction of the rotational forces. There is a progressive meshing, due to the angle of the teeth. The number of teeth engaged at any one time is high, which assures a smooth mesh. The change of direction obtained is therefore smoother and quieter than can be obtained from bevel gearing.
A Right Hand helical crossed gear meshes with another Right Hand gear. The relatively weak yield, due to the axial forces, can cause the transmission to overheat, which can be easily reduced by good lubrication.
You can visually check the angle of the teeth. Place the gear lying flat on a table, if the teeth go up to the right direction, the angle of the teeth is a Right Hand one, if the teeth go up to the left direction, the angle of the teeth is a Left Hand one.
Who are we? - Customer services - International - Terms and conditions - Legal statement - Site map - Contact
copyright © 2001-2006 - Engrenages HPC - All rights reserved - Site optimized for Internet Explorer 6+ and FireFox 1+
Ondrives Ltd - Rino Industries Ltd - Rino Mechanical Components - HPC Ireland
mechanical drives • conveyor parts • power transmission • linear drives
linear motion • rotary motion • gears